How Do I Display the Glossary?
The Glossary is displayed in the left-hand pane of the help window. If the left-hand pane is hidden, use the or
Show/Hide button to display the pane (see Layout of the ClearSCADA Help Window).
To display the Glossary when the Help Contents is on view in the left-hand pane, select the Glossary tab.
You can also use the Show/Hide button to hide the left-hand pane if you no longer require it on view.