Display Default View
            This option is only available if:
- You are accessing the Object menu for a Group, Group Instance, or Group Template.
 - That Group, Group Instance, or Group Template is configured to have a Default View (see Defining a Default View).
 
Select the Display Default View option to display the ‘file object’ (such as a Mimic or Trend) that is configured as the Group, Group Instance, or Group Template’s Default View.
Use the Default View to ascertain further information about the items within the Group and/or access alarm response actions and controls.
Alsosee Display Help View, and see Display Alarm View.