Use the Status Display Buttons
            When accessed from a ViewX Client, a series of buttons is included at the bottom of the Status display:
                
                
            
Use the buttons to perform these activities:
- Copy—This button becomes available for use once you select one or more attributes on the Status display.
        
        
To select the attribute(s) that are of interest, do one of the following:
- Select a single attribute so that it is highlighted.
 - Select a block of attributes—select the first entry that you require, then hold down the Shift key while you select the last entry you require.
 - Select several individual attributes—select the first entry that you require, then hold down the Ctrl key while you make further selection(s).
 
Select the Copy button to place a copy of the highlighted content on your PC’s clipboard. Paste the information from the clipboard into another display or application, as required.
 - Copy All—Select this button to copy the information in the Status display to your PC’s clipboard. Paste the information from the clipboard into another display or application, as required.
 - Refresh—The status values that are shown on the Status display are accurate at the time you select the View Status option. They do not update automatically. Select the Refresh button to update the display to include the data for the current time.
 - Close—Select this button to close the Status display.