Entering and Leaving Persistence

WITS Field Devices support either:

 

Entering a state means that the point value is moving into a different state, away from Normal. A point only enters a new state if its value has been equal to, or beyond the limit threshold for the Persistence duration.

Leaving a state means that the point value is moving into a different state, towards Normal. A point only leaves a state (and therefore enters a new state) if its value has been beyond the limit value (with Hysteresis where applicable) for the Persistence duration.

 

The Device Profile for your Field Device specifies whether the device supports separate Persistence for entering and leaving (see Display a WITS Device Profile).

When you configure WITS database points, the Persistence settings on the Point Form reflect the Persistence supported by your Field Device:

 

For more details on configuring the Persistence durations, see:


Disclaimer

ClearSCADA 2017 R3