Making Changes to WITS Field Device Configuration

If you need to make changes to the configuration of a WITS Field Device (that has already been set up to work with ClearSCADA), you have three options:

For more details, see Using a Configuration Application to Change Field Device Configuration

If the configuration of a Field Device is changed locally, you can choose to overwrite the ClearSCADA configuration with the local configuration. Alternatively, you can overwrite the local configuration with the ClearSCADA configuration, or you can accept that the configuration is different (see Accept Local Configuration).

Further Information

For information on the various ways of configuring a WITS Field Device to interoperate with ClearSCADA for the first time, see WITS Configuration Strategies.


Disclaimer

ClearSCADA 2017 R3