Numeric List of WITS Field Device Attributes

WITS Field Devices support both the common DNP3 Device Attributes and WITS-specific Device Attributes. The topics in this section explain the Device Attributes that are WITS-specific. For more information, see the topics that are listed in the gray footer section at the bottom of this topic. Select the relevant entry to display the topic that you require.

For more information about the common DNP3 Device Attributes, see Numeric List of DNP3 Outstation Device Attributes.

 

ClearSCADA reads the Field Device's Device Attributes and stores them in the database. You can display them in the outstation's Status display. ClearSCADA displays both the common DNP3 attributes and the WITS-specific attributes.

ClearSCADA also:


Disclaimer

ClearSCADA 2017 R3