Using ClearSCADA to Store WITS Device Profiles

In ClearSCADA, you can import, view and export the device profiles that are supplied with your WITS Field Devices (by the device vendor). So you can use ClearSCADA as a repository for your WITS device profile XML files - if you need to use the XML file outside of ClearSCADA, you can export it. The exported XML file is exactly the same as the vendor-supplied XML profile you originally imported.

For more information, please refer to:


Disclaimer

ClearSCADA 2017 R3