Connection Alarm

Associated with: Wonderware Historian database item.

The Connection Alarm attribute indicates the status of the network connection between HCAL and a Wonderware Historian server.

There are two types of connection error:

The ClearSCADA alarm message includes any error message generated by HCAL.

Possible States: Displays one of the ClearSCADA Standard Alarm States.

For information on resolving connection anomalies, see Troubleshooting Wonderware Historian Driver Operation.

Further Information

Connection State


Disclaimer

ClearSCADA 2017 R3