Add a Wonderware eDNA Historian Database Item

You need to add a ClearSCADA Wonderware eDNA Historian database item for the Wonderware eDNA Historian to which you want to export data.

To add a Wonderware eDNA Historian database item:

  1. Display the Database Bar (see Display an Explorer Bar).
  2. In the Database Bar, right-click on the System or Group to which you want to add the new database item.
    A context sensitive menu is displayed.
  3. Select the Create New option.
    A further menu is displayed.
  4. Select the Other option.
    A further menu is displayed.
  5. Select the eDNA Historian option.
    ClearSCADA adds an eDNA Historian database item to the root of the System or to the Group you selected (depending on your selection in step 2). ClearSCADA selects the database item automatically, ready for you to enter its name.
  6. Enter a suitable name for the database item, taking into account the ClearSCADA Naming Restrictions.
  7. Press the Enter key or select another part of the ViewX interface to confirm the entry.

When you have added a database item, you can configure its properties (see Configure a Wonderware eDNA Historian Database Item).


Disclaimer

ClearSCADA 2017 R3