Primary Connection State

Associated with: Wonderware eDNA Historian database item.

The Primary Connection State attribute indicates the status of the primary network connection between eDNALinkMx and the Wonderware eDNA Historian server.

For more about the primary and secondary connections, see Specify the Connection Properties

The possible connection states are:

Further Information

Specify the Connection Properties


Disclaimer

ClearSCADA 2017 R3