Wonderware eDNA Historian Driver-Specific Status Display Attributes

Every item in the ClearSCADA database has its own Status display (also referred to as a View window or View dialog). You view an item's Status display by selecting that item's View Status pick action or menu option. The Status display provides information about the status of the selected item, presenting the information in the form of 'status attributes'. For further information about working with Status displays, see Status Displays.

Example:

The Status display for the Wonderware Historian database item provides information about the status of the network connection between ClearSCADA and Wonderware eDNA Historian.

The database items that are associated with this stand-alone driver support a combination of:

The driver first sets the status information when it uses the eDNALinkMx API to open a connection to the Wonderware eDNA Historian server. Thereafter, the driver polls eDNALinkMx every minute so that it can update the information if a status has changed. It also raises or clears alarms and logs events if required.


Disclaimer

ClearSCADA 2017 R3