Moving Between Intervals on an X-Y Plot

Each X-Y Plot has a Time Line that is configured to represent a specific amount of time. The total time that you can see on an X-Y Plot display at one time is referred to as the interval.

When you display an X-Y Plot, it shows the data for a specific interval. By using the following navigation tools, you can set the X-Y Plot to show the data for different time intervals:


Disclaimer

ClearSCADA 2017 R3