Configure the Axis Display Settings

You can configure various properties that affect the Time axis's appearance. You do this using fields in the Time Axis Properties window (see Configure the Time-Axis Properties).

Use the Axis section of the window to specify these properties:


Disclaimer

ClearSCADA 2017 R3