Configure the Font used for the Axis

You can change the appearance of the font that is used for the Time axis text. You do this using fields in the Time Axis Properties window (see Configure the Time-Axis Properties).

Use the Fonts section of the window to specify the font's appearance:


Disclaimer

ClearSCADA 2017 R3