Configure the X-Y-Z Plot's Title

You can change properties associated with an X-Y-Z Plot's title. You do this using fields in the X-Y-Z Plot Properties window (see Change the Appearance of an X-Y-Z Plot).

Use the Title section of the window to define these properties:

Use the Fonts section of the window to specify the font's appearance:


Disclaimer

ClearSCADA 2017 R3