Configuring X-Y-Z Plots

The topics in this section explain how to create and configure an X-Y-Z Plot. For more information, see the topics that are listed in the gray footer section at the bottom of this topic. Select the relevant entry to display the topic that you require.

To do this, you should:

  1. Create an X-Y-Z Plot.
  2. Display an X-Y-Z Plot in Design Mode.
  3. Configure the X-Axis Properties.
  4. Configure the Y-Axis Properties.
  5. Configure the Time-Axis Properties
  6. Change the Appearance of an X-Y-Z Plot.
  7. Add a Trace to an X-Y-Z Plot.
  8. Configure a Trace.
  9. Add and configure further traces, as required.
  10. Save the changes to the X-Y-Z Plot (see Saving Configuration Changes in the ClearSCADA Guide to Core Configuration).

Users with the relevant permissions will then be able to view and use the X-Y-Z Plot in Run mode (see Using X-Y-Z Plots).


Disclaimer

ClearSCADA 2017 R3