Specify the Quality of the Values that are to be Shown on the Trace

You can specify whether you only want a trace to include values that are of a particular Quality type. A value's 'quality' provides an indication of its reliability. Use the Trace Properties window (see Configure a Trace) to specify the quality of the values that are to be shown on the trace:


Disclaimer

ClearSCADA 2017 R3