Poll Outstations on the Other Channel

This section only applies to:

Providing that:

Heartbeat polling is used to monitor the state of the idle line to an outstation.

A ‘heartbeat’ is a request for a response from the outstation—no processing is performed on the response other than, for instance, to check the framing. Geo SCADA Expert sends the ‘heartbeat' via the channel that the outstation is not currently using. For example, if an outstation’s current channel is B, Geo SCADA Expert will send the heartbeat via channel A. The rate at which Geo SCADA Expert sends heartbeat polls is defined using the channel’s Re-establishment Interval(see Defining Further Scan Parameter Settings for a Direct Channel).

Use the Heartbeat section of the Shared tab to specify whether heartbeat polls are required:

Enabled

Select the Enabled check box to enable heartbeating. The Use Preferred Line check box becomes available for use.

Clear the Enabled check box to disable heartbeating.

Use Preferred Line

Select this check box for an outstation to automatically switch to the preferred line, if heartbeating shows that the preferred line has become healthy. The preferred line is the channel with which an outstation usually communicates with Geo SCADA Expert. An outstation only switches to using its ‘backup’ channel if Geo SCADA Expert detects that the preferred channel has failed. The outstation continues to use the backup channel only until the preferred channel becomes healthy, then switches back to the preferred channel after the delay specified in the Use Preferred Line After n Seconds field.

Use Preferred Line After n Seconds

Specify the time period after which an outstation’s preferred channel is deemed healthy after Geo SCADA Expert has detected that it has failed. Use this setting to help prevent an outstation from performing several switches if the preferred channel fluctuates between healthy and failed. An outstation switches back to using its preferred channel once the channel has been healthy for the length of time specified in this field.


Disclaimer

Geo SCADA Expert 2019