Specify the Fonts used on the Dynagraph

Use the Fonts section of the Dynagraph Properties window to alter the properties of the fonts used on the Dynagraph’s display. You can alter the properties of the font used for:


For each font, you can specify the:

Family

Select the style of lettering from the list of available fonts.

Height

Use the spin box to increase or decrease the size of the lettering as required.

Bold

Select the Bold check box to embolden the specified text, or clear the check box to use normal text. Emboldened text appears as darker and thicker text and is often used for emphasis.

Italic

Select the Italic check box to italicize the specified text, or clear the check box to use normal text. Italicized text appears as leaning text and is often used for emphasis.

Further Information

Specify the Labels Used for the Dynagraph’s Axes.


Disclaimer

Geo SCADA Expert 2019