Adjust the Configuration of any Points that Cause a High Load

A possible cause of deficient performance on a Geo SCADA Expert system is that of inadequate client performance (see Diagnose Client Performance Problems). One of the causes of inadequate performance is high load on the server.

You can use the statistics that are shown in Lists and Status displays to identify any Generic Modbus controllers that are causing a high loading on the Geo SCADA Expert system.

For those controllers that have a high load, use the Points List to identify the point(s) that are causing the high load.

High load is typically caused by a point updating at too frequent a rate.

  1. Check the Retrieval Interval that the point is using (see Configure Common Point Properties). If this is causing the server to update the current point value at too frequent a rate, you might need to:
  2. If the point is on a controller that has a direct connection to the server, check the Scan Group (Confidence Interval) that the point is using (see Configure Common Point Properties). If this is causing the server to update the current point value at too frequent a rate, you might need to:
  3. If the point is an Analog point, ensure that the Significant Change feature is enabled (see Define the Criteria for a Significant Change in Value).
  4. If the point is an Analog point with Significant Change enabled, you might need to increase the Significant Change deadband—the amount by which the point value has to change in order for the value to be updated in the Geo SCADA Expert database (see Define the Criteria for a Significant Change in Value).
  5. If fleeting changes in value are causing a high load, you might want to increase the Persistence settings for the point (see Use Persistence to Stop Fleeting Changes in Value from Changing a Point State). However, a sudden increase in momentary changes in state might indicate an abnormal condition elsewhere. If this occurs, check the controller, plant, and instrumentation to see whether an underlying hardware problem is causing the sudden increase.
  6. If none of the above checks and configuration changes have cleared the high load caused by the point, check the following equipment for any faults:
    • Controller hardware
    • Plant
    • Instrumentation.

Disclaimer

Geo SCADA Expert 2019