Configuring an Advanced Modbus Set

The Advanced Modbus driver supports four types of Advanced Modbus outstation set:

In each case, you specify the features for a set by using the fields on the appropriate Advanced Modbus Outstation Set Form.

Each Form has several tabs.

Use the Modbus tab to:

For Advanced Modbus Outstation Sets other than PSTN, also use the Modbus tab to:

Properties on other tabs are common to outstation sets on many advanced drivers—for information, see Tabs on Outstation Set Forms.


Disclaimer

Geo SCADA Expert 2019