Modbus Function Codes Supported by the Geo SCADA Expert Advanced Modbus Driver

The Geo SCADA Expert Advanced Modbus Driver supports several Modbus function codes, enabling it to read and write data on Modbus devices. The standard function codes that the Geo SCADA Expert Advanced Modbus Driver supports are:

Modbus Function Code Functionality Maximum Number of Registers that can be Read or Written to using a Single Command

FC1

Read Coil Status

2000

FC2

Read Input Discretes

2000

FC3

Read Multiple Registers

125

FC4

Read Input Registers

125

FC5

Write Single Coil

1

FC6

Write Single Register

1

FC15

Write Multiple Coils

3

FC16

Write Multiple Registers

4

FC22

Mask Write Register

1

The actual maximum number of registers or coils requested in a read might be smaller than the number listed above. This will occur if a channel’s Maximum Packet Size has been reduced (see Specify the Required Modbus Protocol and Packet Size).

As only a limited number of Modbus controllers support FC22, this function is made optional on Generic Modbus Digital Output Points in Geo SCADA Expert (see Specify the Type of Control Operation).

Similarly, as some Modbus controllers do not support both FC6 and FC16, each generic controller’s Register Write function has to be specified in Geo SCADA Expert (see Specify the Register Write Function).


Disclaimer

Geo SCADA Expert 2019