Specify the Frequency with which Communications Statistics are Updated

Use the Communication Statistic Updates section on the Remote Connection tab to define how often the communication statistics are updated. You can view the statistics on the remote connection’s Status display.

Example:

The Communication Statistic Updates properties for a remote connection are configured as:

Interval = 1M
Offset = 30S

If the time is currently 00:00:00, the next Communications Statistics update will occur at 00:00:30, followed by another update at 00:01:30, then another update at 00:02:30, and so on, at 1-minute intervals offset to 30-seconds past each minute.


Disclaimer

Geo SCADA Expert 2019