Configure Point Sampling (OPC DA 3.0 only)

The Sampling section on an Advanced OPC Point Form allows you to configure the rate at which individual items within a group are obtained from the underlying device. Using the properties in this section does not affect the group update rate associated with the items.

Point sampling is only available for some OPC Servers that support and are configured to use the OPC DA 3.0 protocol, (see Configure the Advanced OPC Server).

Further Information

Configure an Advanced OPC Group


Disclaimer

Geo SCADA Expert 2019