Asynchronous Polling

When the Read Type or Write Type within the specified Advanced OPC server(s) is configured as Asynchronous (see Configure the Advanced OPC Server), you need to complete the Asynchronous section within the Advanced OPC Group associated with the server.

Further Information

Configure the Advanced OPC Server

Configure other properties on an Advanced OPC Group Form: see Configure an Advanced OPC Group.

see Configure OPC DA Server Properties


Disclaimer

Geo SCADA Expert 2019