Synchronous Polling

You can configure synchronous polling in Advance OPC groups and/or individual points. If you intend to use synchronous polling to request data you need to enable and complete the Synchronous Pollingsections on the relevant Advanced OPC configuration Forms.

This section only applies to setups in which the Read Type has been set to Synchronous on the Advanced OPC Servers, (see Configure OPC DA Server Properties).

Synchronous Polling for a group

Use the fields within the Synchronous Polling section of an Advanced OPC Group Form to specify the polling that Geo SCADA Expert is to apply to all active points within that Group.

Synchronous Polling for a Point

Use the fields within the Synchronous Polling section on an Advanced OPC Point Form to specify polling that Geo SCADA Expert is to apply to that particular point. The individual point polling occurs in addition to the group polls.

To configure synchronous polling complete the following fields:

Further Information

Configure an Advanced OPC Group

Points Used on Advanced OPC Groups


Disclaimer

Geo SCADA Expert 2019