Trio Radio Series Supported by the Advanced Trio Diagnostics Driver

You can use Geo SCADA Expert's Advanced Trio Diagnostics driver to retrieve diagnostics data from several series of Trio radio. The type of diagnostics data that Geo SCADA Expert can retrieve from each radio varies, depending on the radio series and the type of radio unit.

The Advanced Trio Diagnostics driver provides support for retrieving diagnostics data from the following series of Trio radio:

Trio
Radio
Auto-Diagnostics Dual-Base
Radios
Control of Digital Output Relays
Comments

D Series

   

D Series radios are capable of providing feedback on fewer diagnostics parameters than other radio series supported by the Trio Diagnostics driver. You retrieve each of the diagnostics parameters using a Trio Diagnostics Analog point.

D Series radios provide a subset of other features supported by later series of Trio radios.

E Series

The E, J, K, and M Series of Trio radios use a diagnostics protocol that provides additional functionality to D Series radios.

The actual items of diagnostics data that can be retrieved from each radio vary, depending on the radio series and type of unit (for example, a base station, repeater station, or remote data radio).

J Series

   

K Series

   

M Series

   
Q Series

Q series radios provide different functionality to other radio series. They also provide enhanced security features and faster data speeds.

You can retrieve Q series diagnostics data using either the Geo SCADA Expert SNMP driver, or the Advanced Trio Diagnostics driver.

The actual items of diagnostics data that can be retrieved from each radio vary, depending on the type of radio unit (for example, a base station, or remote data radio).


Disclaimer

Geo SCADA Expert 2019