Add an Action Roster

Before you can redirect an item’s alarms on a roster basis, you need to add and configure an Action Roster.

To add an Action Roster:

  1. Right-click on the System or Group to which you want to add the roster (this might be a separate Group for storing redirection actions).
    A context sensitive menu is displayed.
  2. Select the Create New option.
    A further menu is displayed.
  3. Select the Alarm Redirection option.
    A further menu is displayed.
  4. Select the Action Roster option.
    An Action Roster is added to the system. It is selected automatically, ready for you to enter its name.
  5. Enter a suitable name for the Action Roster (see Naming Restrictions in the Geo SCADA Expert Guide to Core Configuration).
  6. Select another part of the interface or press the ENTER key to confirm the entry.

When you have added an Action Roster, you need to Display and Configure Properties on the Action Roster Form.


Disclaimer

Geo SCADA Expert 2019