Alarm Redirection and Suppressed Alarms

Alarm redirections do not trigger for any item for which alarms are suppressed. An alarm can be suppressed (omitted from any alarm displays) due to an alarm being raised on ‘parent’ item.

Should the parent alarm clear, any alarms that were suppressed because of that alarm become unsuppressed if they still exist. Once an alarm becomes unsuppressed, it appears on any alarm displays and Geo SCADA Expert triggers any associated alarm redirections in the usual way.

Further Information

Alarm Suppression: see Alarm Suppression in the Geo SCADA Expert Guide to Alarms.

Configure any Alarm Suppression Requirements in the Geo SCADA Expert Guide to Core Configuration.


Disclaimer

Geo SCADA Expert 2019