Specify whether Users can Resize the Columns on the Alarm Banner

By default, the Alarm Banner uses columns that are a fixed size that cannot be changed by dragging the column lines. But by using the Option window, you can provide users with the ability to change the Alarm Banner column size as required.

To define whether users can resize the columns on the Alarm Banner:

  1. Log on via a user account that has the Configure Options permission, and then display the Options window.
  2. Select the Alarms and Events tab.
  3. Either:

    Or:

Allow Column Resizing is clear by default.

To apply the Allow Column Resizing setting that you have chosen, select the Option window’s OK button. The settings will be applied to the ViewX client on which you defined the changes.


Disclaimer

Geo SCADA Expert 2019