Configure Aquis Server Item URL Parameters

When configuring a hyperlink Pick Action for an Aquis Server database item within a mimic you can add parameters to the URL to define the display and the type of data displayed, (see Hyperlinks that Define Values for Mimic Parameters on a Target Mimic).

You can use the following parameters with the hyperlink URL for the Aquis Serverdatabase item:

Examples:

The following examples illustrate the use of the parameters in the hyperlink Pick Action:


Disclaimer

Geo SCADA Expert 2019