Check the Status of a Third Party OLEDB Client - System Connection

You can use the Server Status Tool to view the status of the Third Party OLEDB client - system connection (see Run the Server Status Tool in the Geo SCADA Expert Guide to the Server Status Tool).

To view the status of a Third Party OLEDB client - system connection, you need to view the Server>Links status settings. The Server Links settings provide information about every client - system connection including the OLEDB connections.

The Links information includes:

For more information, see Links (Server) in the Geo SCADA Expert Guide to the Server Status Tool.


Disclaimer

Geo SCADA Expert 2019