Failed Third Party OPC Client - System Connections

If the Third Party OPC client - system connection cannot be established, you will be unable to connect to Geo SCADA Expert from the Third Party OPC client application.

A connection may fail to establish if:

The Third Party OPC Client - system connection works in the same way as a ViewX - system except that it uses a different license and it requires Data Access components to be installed on the OPC client PC. As such, the firewall rules for Third Party OPC client - system connections are the same as those for ViewX - system connections.

Further Information

Firewall Settings for Client - System and Server Advise Connections.


Disclaimer

Geo SCADA Expert 2019