Third Party ODBC Client - System Connections

You can use data from the Geo SCADA Expert database in Third Party ODBC client applications such as SAP Crystal Reports and Microsoft Excel. The data can be used in reports, spread sheets, other databases, and so on.

To use a Third Party ODBC client application to access your Geo SCADA Expert system, you need to install the Data Access components of Geo SCADA Expert on the same computer as the Third Party ODBC client application(s). This is because the Third Party ODBC applications need to use the Data Access components to connect to a Geo SCADA Expert database.

We refer to computers that run Third Party ODBC applications and have Data Access components installed as Third Party ODBC Clients.

Communications between the Geo SCADA Expert serverand the Data Access components installed on the ODBC client work in a similar way as communications between a ViewX client and Geo SCADA Expert server. The only difference is that with an ODBC client, there is a single link that is used for client to server messages and server responses. There is no server advise link for unsolicited messages from the server. For more information, Understanding Client - System and Server Advise Connections.

To allow a Third Party ODBC client to access the Geo SCADA Expert system, the Data Access components have to be:

To connect a computer that runs Third Party ODBC applications to the server, you can either:

Or:


Disclaimer

Geo SCADA Expert 2019