Original WebX and XML Client - System Connections

ATTENTION: This section and associated topics apply to the Original WebX client only.

Geo SCADA Expert supports remote access via Original WebX clients and third-party XML clients. Original WebX clients  are client PCs that run the WebX application supplied by Schneider Electric and third-party XML clients are client PCs that are running an XML application not supplied by Schneider Electric. Both types of client provide remote access to your system by connecting, via Internet or Intranet, to a web server that is installed on the Geo SCADA Expert server.

Original WebX clients and third-party XML clients can be used at any location where secure network access is provided and are easy to set up.

However, there are some limitations with Original WebX and XML clients:

In the following sections, we describe how Original WebX/XML client - system connections work and explain how to connect to Geo SCADA Expert via Original WebX/XML.


Disclaimer

Geo SCADA Expert 2019