Add Rows to an Empty Data Grid
            It is possible to delete all of the rows in a Data Grid, such that the Data Grid only contains field headings:
                
            
To add a row to such a Data Grid, either:
- Right-click on the blank heading cell to the left of the first field heading.
A context-sensitive menu is displayed.
 - Select the Insert option.
A row is inserted below the heading cells. 
To add further rows, either repeat the above procedure, or see Add Additional Rows to a Data Grid.