Add a Data Grid

To add a Data Grid to the Geo SCADA Expert database:

  1. Display the Database Bar (see Display an Explorer Bar).
  2. In the Database Bar, right-click on the System or Group for which you want to add a Data Grid.
    A context sensitive menu is displayed.
  3. Select the Create New option.
    A further menu is displayed.
  4. Select the Tables and Grids option.
    A further menu is displayed.
  5. Select the Data Grid option.
    A Data Grid is added to the root of the System or to the selected Group (depending on your selection in step 2). It is selected automatically, ready for you to enter its name.
  6. Enter a suitable name for the item (taking into account the Geo SCADA Expert Naming Restrictions).
  7. Press the Enter key or select another part of the ViewX interface to confirm the entry.

When you have added a Data Grid to the system, you can then Configure the Properties on the Data Grid Form, or Edit a Data Grid and add entries to that Grid.


Disclaimer

Geo SCADA Expert 2019