Column Headings for other Types of Value Map

These column headings are displayed for Value Maps other than BIT Value Maps:

Example:

A floating-point analog value has been configured to have its Data Type converted from REAL to WORD when mapped to a Value Map. To avoid the analog value being truncated when read by the driver, the value is scaled on the Value Map. The default settings are used, whereby the point’s 0 to 100 scale is converted to 0 to 65535 at the Slave.

At the Slave’s master, the point value is reverse-scaled, whereby the 0 to 65535 scale is converted to a scale of 0 to 100.


Disclaimer

Geo SCADA Expert 2019