Define the Acceptable Number of Event Journal Records

Use the Event Journal tab on the Root Group Form to manage number of acceptable Event Journal records. There are two sections provided to manage these records.

If the limits are increased on the root group properties they do not take immediately and suppression will continue at the previous limits (for items with counts above limits) until a new hour boundary, see Unsuppress Event Logging.

When the Event Journal becomes overactive:

Further Information

Historic Types and Streams

Defining Severities


Disclaimer

Geo SCADA Expert 2019