Dial In Disabled

Associated with: Outstations that communicate via PSTN, including outstations with PSTN fallback

The Dial In Disabled state is indicated by a brown foreground color.

The color indicates that a PSTN outstation is prevented from dialing in to the server (calls from the server to the outstation are not stopped). Dial in is disabled using the Disable Dial In pick action and enabled using the Enable Dial In pick action.


Disclaimer

Geo SCADA Expert 2019