Display the Schedule in Design Mode

To add actions to a Schedule, or to add events (other than to a Simple Schedule), you need to display that Schedule in Design mode.

To display a Schedule in Design mode, either:

  1. Display the Database Bar (see Display an Explorer Bar).
  2. Double-click on the required Schedule entry in the Database Bar (if you are logged on as a user that has the Double Click Edits Documents feature enabled).

or:

  1. Display the Database Bar (see Display an Explorer Bar).
  2. Right-click on the Schedule in the Database Bar.
    A context sensitive menu is displayed.
  3. Select the Edit Schedule option.

The Schedule is displayed in Design mode. The actual display varies, depending on the type of Schedule (see Types of Schedule Display).


Disclaimer

Geo SCADA Expert 2019