Example Basic Data Set Configuration

You can use Data Sets to add ‘custom’ tables to your database. You use the Data Sets to collate, organize and summarize data from elsewhere in the database, in a tabular format that can be queried from, for example, a List or a Report. You use Data Sets, rather than Data Grids, if your database is 'modular' and you want to collate data from database items in multiple similarly structured Groups. You use Data Set Rows to define the data that you want to obtain from each Group. You associate the Data Set Rows with the Data Set. Whenever you make a further copy of a Group that contains a Data Set Row, a record is automatically added to the Data Set's table for that new Group.

The example below demonstrates the key steps in configuring a Data Set and associated Data Set Rows in 'normal' Groups, although similar steps apply if the Data Set Row is in a Group Template. For an example that further demonstrates the benefits of configuring Data Set Rows in Group Templates, see Example Template Data Set Configuration.

Example:

You configure a Data Set database item using a configuration Form and an Editor.

Further Information

Expressions: see the Geo SCADA Expert Guide to Expressions.


Disclaimer

Geo SCADA Expert 2019