Future Data

Associated with: Points

The Future Data state is indicated by a green-blue foreground color, by default.

The color is used on the Historic List to indicate that the time stamp for the data is inaccurate in as much as the clock for the outstation, or PLC on which the point is located, had drifted forwards by more than the acceptable clock drift.

The Future Data setting is specified in the Points section of the Geo SCADA Expert Server Configuration Tool (see Define the Maximum Outstation Clock Drift).


Disclaimer

Geo SCADA Expert 2019