Locate the Configuration Property to Which a Message Relates

If a message in the Messages window indicates that a database item has invalid or conflicting information, you can locate the configuration property to which the message relates. To do this, either:

  1. Right-click on the message in the Messages window.
    A context-sensitive menu is displayed.
  2. Select the Go To Problem option.
    Providing that your User Account is assigned the necessary permissions and access, Geo SCADA Expert displays the configuration Form for the relevant database item. The cursor is positioned at the configuration property to which the message relates

    Or:

The Go To Problem option is only available with a message that relates to a specific configuration property.


Disclaimer

Geo SCADA Expert 2019