Overrun Count

Associated with: Master Station Accumulators that use a Continuous reset method

This status attribute indicates whether Geo SCADA Expert has omitted to process the Accumulator total within the configured End of Period Reset or Timed Report intervals. The Overrun Count is only likely to increment in exceptional circumstances—for example, if an extremely short Interval (such as 1 Second) is specified, but Geo SCADA Expert was unable to process the Accumulator’s value at the required time due to the system being exceptionally busy.

An Overrun Count of 0 (zero) indicates that no counts have overrun since the Accumulator’s configuration was last saved.


Disclaimer

Geo SCADA Expert 2019