Parameters

Parameters are stored as configuration in the Geo SCADA Expert database. Parameters are intended to store static values and can be used as an alternative to custom fields.

Create and configure a Parameter on your system if you require:

If using String Parameters, consider using a Parameter Table, rather than a series of String Parameters, if a set of up to four String Parameters is required.

Further Information

Add a Parameter

Configure a Parameter

Example Configuration

Importing and Exporting Database Items


Disclaimer

Geo SCADA Expert 2019