Printing

Geo SCADA Expert provides you with the facility to print a variety of data output. You can configure printing to be done manually or to occur automatically. The following is a list of features with which you can use the print facility:

There are two printing options available for various features within Geo SCADA Expert:

In Microsoft® Windows®, you can only access those printers that are associated with your Windows user accounts. The Geo SCADA Expert server runs as a service, so a system administrator needs to specify a Windows user account in the Geo SCADA Expert server configuration to allow the Geo SCADA Expert server to access the required printers, see Printer Settings.


Disclaimer

Geo SCADA Expert 2019