Specify the Database Item that a Link Parameter is to Reference

Use the Link tab on a Link Parameter’s Form to specify the Geo SCADA Expert database item that the Parameter is to reference.

To specify the item, select the browse button to the right of the Object field. A Reference browse window is displayed. Select the required database item from the window.

You can use a Link Parameter to reference any item in the database. For an example that demonstrates how you might use Link Parameters in Geo SCADA Expert, see Use Link Parameters to Enable the Instances of a Mimic to Reference Different Locations.


Disclaimer

Geo SCADA Expert 2019