Specify the String Parameters that a Parameter Table is to Store

Use Parameter Tables to store up to four interconnected strings. To store only single strings, consider using String Parameters (see Specify a Single String Parameter).

This section describes the fields on the Parameter Table tab of the Parameter Table Form.

Use the four Parameter fields on the tab to specify up to four strings that the Parameter Table is to store.


In each field, you can specify an alphanumeric string of up to 128 characters, including spaces.

Example:

On a particular Geo SCADA Expert system, Parameter Tables are used to store three strings. The strings specify a site name, an operator name, and a contact number.

The system is configured to display the parameters on the relevant Mimics and reports.


Disclaimer

Geo SCADA Expert 2019