Specify the Total Lock Time per Minute Alarm
The Total Lock Time per Minute Alarm section allows you to configure the alarm settings when the last minutes average of total lock usage exceeds configurable thresholds.
Use this field to define the percentage total lock time that needs to occur to raise a High Warning alarm, the default setting is 80%.
Use this combo box to define the severity of the High Warning Alarm. For more information on severities, see Defining Severities.
Use this field to define the percentage total lock time that needs to occur to raise a High High Warning alarm, the default setting is 90%.
Use this combo box to define the severity of the High High Warning alarm. For more information on severities, see Defining Severities.
When the server starts up there is a lot of activity related to the database, which would cause Lock Usage alarm thresholds to be exceeded and alarms generated. Use this field to define a period at start-up when these alarms are suppressed. The default setting is 15 minutes.
This field is only displayed if the Area of Interest feature is enabled on your system. Use the field to specify the Area of Interest with which the item's alarms and events are to be associated (see Assign a Different Area of Interest to an Item's Alarms and Events). For further information about the Area of Interest feature, see Restrict Alarm and Event Access to Specific Areas of Interest.
In addition to an alarm appearing in the Alarm Banner a warning appears in the Server Status General Information window, see General Status - Information.
WARNING - Database Lock Usage WAS above a CONFIGURED HIGH LIMIT (Alarmed Value: 60.3742% at '18-MAY-2018 14:26:15.737')
Please examine system activity in the Performance pages.